2016-07-27 2:17 PM
Hello, We are using lsm6ds3 sensor by connecting to STM32F103 controller through I2C communication. Over I2C to read both X and G Raw data taking around 800uSeconds over 400K speed.
In one of my new project, needed both X&G raw values for every millisecond.For fast reading, thinking to use SPI communication instead of I2C communication. Provided examples with in X-CUBE-MEMS1 are based off I2C, is there example any examples for SPI connection?Regards,Jim #lsm6ds3 #stm32f10x #4-wired-spi2016-07-29 12:11 AM
Hello Tim,
Unfortunatelly X-CUBE-MEMS1 package uses the IKS01A1 MEMS Shield expansion board which does not support SPI at all so therefore there is no sample code for SPI.Best regards,Petr