2013-01-11 09:05 AM
Section 6.2 of the data sheet says that ''SPC,SDI,SDO are common'' however there are 2 different SDO pins, SDO_A and SDO_G. Has anyone tried connecting the two SDO pins on the target board?
Does anyone know if I2C mode always active when the CSx pin is HI? If so how do you prevent the I2C module for erroneously receiving a command from other devices that may be operating on the SPI bus? Thanks2013-05-27 07:22 AM
Any update?
2013-06-06 12:50 AM
Hi
I have the same
doubt, the
datasheet
is confusing
on this issue.
Furthermore
evaluation
board
STEVAL
-
MKI109V2and
''Unico
GUI''
using
I2C
protocol
. Best regards2015-02-20 09:40 AM