cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSV320X: Confirmation on Free-Fall Interrupt Mapping (INT10)

Ahilesh_Krishna
Associate II

Hello Team,

We are using SensorTile.box Pro with the STEVAL-MKI251A (LSM6DSV320X) adapter board and MEMS Studio version 2.2.0. Flashed the sensor tile box pro with the DataLogExtended.bin firmware which is available in the MEMS Studio

We have logged accelerometer Low-G and High-G data at 1.9 kHz. Additionally, we enabled and monitored interrupts from INT1 to INT10 during the test.

We observed that only INT10 shows an output value of 1, while all other interrupts remain inactive.

Could you please confirm from your side whether INT10 = 1 corresponds to the Free-Fall interrupt for this sensor configuration? Also, kindly let us know if this behavior is expected when using MEMS Studio 2.2.0 with SensorTile.box Pro and the STEVAL-MKI251A.

Thank you for your support.

Best regards,
Ahilesh

3 REPLIES 3
Federica Bossi
ST Employee

Hi @Ahilesh_Krishna ,

Can you do a register dump? it can be obtained with MEMS Studio in the save configuration section.
In addition, what do you mean by INT10?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ahilesh_Krishna
Associate II

Hi @Federica Bossi 

Thanks for your reply.

While logging the High g and Low g accelerometer sensor, in the csv file i could see the Interrupts printed from INT1 ro INT10. Only in INT10 i could see the value changing from 0 to 1, Would like to confirm that this is the free fall detection interrupt. Hereby attaching the log for reference. 

Miroslav BATEK
ST Employee

Hello @Ahilesh_Krishna,

The logical signal Interrupt 9 in MEMS Studio reflects INT1 of the sensor connected in DIL24 socket in your case LSM6DSV320X and Interrupt 10 reflects INT2 of the sensor.
So it depends on your sensor configuration, whether the free fall detection interrupt is routed to INT1 or INT2, both options are possible. You can test in on the Acc Interrupt page.

MEMS Studio_Interrupt_LSM6DSV320X.png