2021-01-28 03:59 AM
Hi.
According to the DS of the LPS33W - the Reflow profile should be according to JEDEC J-STD-020 , with no actual determination of the profile.
we had several boards assembled , and with very little force applied, the sensor disintegrated - the metal part from the plastic socket.
I suspect it might be the reflow profile that weaken the glue and caused this disintegration.
Is there a recommended profile for the LPS33W?
We have used before that the STEVAL-MKI205V1 - which is the LPS33W EVB ,
And had no such issue.
The pic below is of an actual reflow performed on the boards.
Thanks.
Solved! Go to Solution.
2021-03-17 10:09 AM
Hi @SGano.1 ,
I suggest you to contact a representative from your region the from the st.com contact page, to get more support and internal visibility -and eventually escalation- on this quality issue.
-Eleon
2021-01-29 07:03 AM
Hi @SGano.1 ,
Which soldering technique are you using (convection / vapor phase)?
The profile looks overall good, especially in the first part.
However, comparing it with the one in AN4450 application note (Hardware and software guidelines for use of LPS25H pressure sensor... well it's another pressure sensor but the soldering profiles are all very similar):
I would suggest you to increase the speed of cooling ramp from 1°C / sec as in your case to at least 2°C/4°C / sec as in the above picture.
Moreover, in AN4450 application note you can find other considerations to be taken into account:
In using non self-cleaning solder paste, proper board washing after soldering must be carried out to remove any possible sources of leakage between pads due to flux residues. However, take care not to perform the cleaning process on top of the pressure sensor.
Let me know if you can try the modified solder profile.
-Eleon
2021-01-31 12:05 AM
Thanks Eleon.
I will check wit my SMT vendor for profile modification.
Is there another explanation Why would the LPS33W Disintegrate that way?
2021-02-01 01:30 AM
Hi @SGano.1 ,
I checked internally and it could be that -in rare cases- due to tight tolerances at mounting on the specific application platform, the cap could receive lateral stresses and worse its adherence.
Which is the failure rate of this issue? Do you have other components near the sensor on the board? And could you estimate the force you apply while you are soldering the device?
If you could better tune the soldering / mounting process, you should solve the issue since it only occurs at the high soldering temperatures in specific "surrounding" conditions.
-Eleon
2021-02-01 05:49 AM
Hi @Eleon BORLINI ,
All the LPS33W that were assembled, have Disintegrated.
Just a little touch disintegrates the Sensors.
Moreover - after a rework process for replacing the faulty component - two components gave false data (80mBar ambient pressure instead of 1010mBar, and false data of temperature too.
The I2C comm is OK and the sensor communicates with the uC- but gives the false data.
Attached another pic from another Board.
2021-02-02 11:49 PM
Hi @SGano.1 ,
but does the chip decap during the soldering process or after?
-Eleon
2021-02-03 03:56 AM
Hi @Eleon BORLINI ,
This happens after the soldering.
After it comes out of the SMT,
It looks intact, even though it is held only by the Gel inside.
2021-02-03 04:19 AM
So it is something happening during the soldering process that is weakening the capping for some reason...
Do you perform an IQC to check the integrity of the devices before soldering?
Could you try modifying the cooling step of the reflow profile as suggested above?
-Eleon
2021-02-12 02:34 AM
Hi @SGano.1 ,
did you eventually manage to try to slow down the cooling ramp of the soldering profile?
-Eleon
2021-02-14 04:36 AM
Hi @Eleon BORLINI
We have not performed another SMT assembly yet.
We had all our boards fitted with the LPS33W reworked,
and so far so good.
Didn't you mean a faster cooling ramp by
"I would suggest you to increase the speed of cooling ramp from 1°C / sec as in your case to at least 2°C/4°C / sec as in the above picture" ?