cancel
Showing results for 
Search instead for 
Did you mean: 

lps22hb i2c interface(erorrs)

Not applicable

Hello, 

We want to operate the LPS22HB pressure sensor with the i2c protocol. The pin legs of the sensor are connected to the SCL - SDA 4.7k ohm pull-up resistors. Sa0/GND   Csi / 3.3  RES / GND. This is how connections are made. This way we can't get data from the sensor. What is the reason of this?

 

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Hi @Sinoplu57 ,

In alternative you can try to reduce the pull up resistances, for example you can use 2.2kOhm.

Let me know if this solves.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.