cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DHTR interrupt pins

bojan
Associate II
Posted on May 25, 2016 at 14:09

Hello guys,

I'm planing to use LIS3DHTR accelerometer in my next project. There is one thing (for the moment :-)) that is bothering me:

The default state of the INT1 and INT2 pins is not explicitly indicated within a datasheet (at least I could not find it). I'm curious to know what is default state of the INT1/INT2 pins and what is the state of those pins when the interrupt occurs?

Is this parameter (the state during the interrupt) configurable through I2C/SPI interface or there is just one default value?

Thanks in advance for your time and effort.

Sincerely,

Bojan.

#lis3dh #lis3dh-interrupt
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on June 30, 2016 at 09:48

Hello Bojan,

For interrupt configuration please refer to application note AN3308

http://www.st.com/content/st_com/en/products/mems-and-sensors/accelerometers/lis3dh.html

.

The default state of INT1 and INT2 pins is Low, when the interrupt occurs the pin goes High.

This parameter can be configured in CTRL_REG6 (bit 1 – H_LACTIVE).

Best regards

Miroslav