cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DE/H RES pin

maciek
Associate II
Posted on December 01, 2017 at 11:20

Hello,

I would like to ask what is 'RES' pin in LIS3DH and LIS3DE? The only informtion is that it should be connected to the ground. Is it hardware reset which is activated with high state?

2 REPLIES 2
Aaron Derbyshire
Associate II
Posted on December 01, 2017 at 17:00

RES typically refers to RESERVED. However, this doesn't mean that the pin may not have a manufacturing purpose but that's not something I imagine they would share on a public forum......

Posted on December 01, 2017 at 17:13

Yes,

Derbyshire.Aaron

‌ is right the pin is RESERVED and must be connected as it is stated in the datasheet. It is NOT reset pin.

These pins might be used in production but are useless for end users.