2021-06-29 7:22 AM
HI :) , I want to exploit the option (if exists) to read the fifo buffer and write to it simultaneously .
meaning the device writes to the buffer and gets to the 11th sample (for ex.) , when I ask to read the data I will get the 0-11 samples and meanwhile the device will keep writing the 12th sample and on..
can I do it?
2021-07-26 12:10 AM
Yes, your SPI master. You should be able to change the communication frequency increasing it up to 10MHz.
If you read 32 data with that speed, the reading will take 32*16 bit *1/10MHz = 50 us << 1/12.5Hz = 80ms which is the speed of your ODR / FIFO filling rate.
-Eleon