cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DH12 accelerometer SPI Interface Clock Speed

MykolaLevun
Associate III

Hello,

 

What is the maximum data transfer rate over the SPI interface for the LIS2DH12 accelometer? The datasheet doesn't say anything about this. About the I2C interface it is said that it can operate in standard mode (up to 100 kHz) and fast mode (up to 400 kHz). But nothing is said about the SPI interface.

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @MykolaLevun ,

Please refer to page 13 of the datasheet:

FedericaBossi_1-1707306380982.png

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @MykolaLevun ,

Please refer to page 13 of the datasheet:

FedericaBossi_1-1707306380982.png

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thank you!