cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DH : False Interrupt_2 detection when device in steady state

NPate.19
Associate

We are using LIS2DH to detection rotation (Interrupt 2).

Configure threshold level for interrupt2 is 750mg and test at two different duration 200ms and 1000ms.

Is there any configuration issue?

1 REPLY 1
Miroslav BATEK
ST Employee

What is the format of attached files?

I need to know the sensor configuration and what exactly you want to detect.