2021-01-21 9:08 AM
I am trying to set up a self test process for an assembly including an LIS2DE12. The device works normally when I tilt and invert it. When I try to put it in to self-test mode by writing either 02h or 04h to CTRL_REG4 the readings are the same as with 00h written to CTRL_REG4.
I initially tried using the process for the LIS3DH on Page 57 of AN3308 but that says to write 80h to CTRL_REG4, which does not seem to be valid because that would set the BDU bit to 1, not valid for an 8 bit part, and not set either of the self test bits.
Can someone please shed some light on whether the self-test function is available with the LIS2DE12 and what I can expect from it.
Thanks in advance,
Rob
Solved! Go to Solution.
2021-01-22 9:13 AM
Hello again Eleon,
I have found the problem and now getting good consistent results in self test mode. I had forgotten to set the write bit used by the state engine that controls the SMBUS in the MCU I am using. I still can't get it to work with the Arduino but that doesn't matter.
Results I am getting, with the device sitting at an angle:
$ normal mode CTRL_REG4 = 00h
FD 19 3B
FE 19 3A
FF 19 3A
FE 18 3A
FE 18 3B
! self test mode CTRL_REG4 = 04h
E1 FD 51
E1 FB 50
E2 FD 4F
E2 FC 51
E2 FC 50
E3 FD 50
$ normal mode CTRL_REG4 = 00h
FE 19 39
FE 18 3A
FE 19 3A
Thanks again,
Rob
2021-01-22 12:53 AM
Hi Rob @RKeit.1 ,
I suggest you to check also the C code implementing the self-test procedure for the LIS2DE12 that you can find on Github at this link --> lis2de12_self_test.c
This procedure is a little long, so it might be useful to have a double check on that code, besides the procedure described in the AN3308 p.57 (which is for the LIS3DH )
Please let me know if the code is useful for your purposes.
-Eleon
2021-01-22 2:26 AM
Hello Eleon,
Thank you for your answer. That gives me some clues. One thing I am still unsure of is the magnitude of the variations in readings during self test. Is it like a few LSBs or bigger? Does it occur on all axes? I know the answers are probably in the documentation but I have winter brain fog.
I see the term mg used. Is that milli-gravity? If so then it could be too small for the readings to be noticeable with only 8 bits or buried in the noise from my wobbly desk. I am working with an 8 bit MCU to develop the test process so I am just looking at the raw X, Y and Z bytes.
Also, does the device stay in self-test mode indefinitely, until CTRL_REG4 is re-written?
Rob
2021-01-22 9:13 AM
Hello again Eleon,
I have found the problem and now getting good consistent results in self test mode. I had forgotten to set the write bit used by the state engine that controls the SMBUS in the MCU I am using. I still can't get it to work with the Arduino but that doesn't matter.
Results I am getting, with the device sitting at an angle:
$ normal mode CTRL_REG4 = 00h
FD 19 3B
FE 19 3A
FF 19 3A
FE 18 3A
FE 18 3B
! self test mode CTRL_REG4 = 04h
E1 FD 51
E1 FB 50
E2 FD 4F
E2 FC 51
E2 FC 50
E3 FD 50
$ normal mode CTRL_REG4 = 00h
FE 19 39
FE 18 3A
FE 19 3A
Thanks again,
Rob
2021-01-24 11:42 PM
Very good @RKeit.1 !
Remember also to use the LSB-to-milli "g" (meaning 1 gravity acceleration 9.81m/s^2 divided by 1000) conversion formulas. This is the standard magnitude for computing the acceleration with an accelerometer. The formula in the FS = 2g case is (source: lis2de12_reg.c)
float_t lis2de12_from_fs2_to_mg(int16_t lsb)
{
return ( (float_t)lsb / 256.0f ) * 15.6f;
}-Eleon
2021-01-25 1:58 AM
I do all that on the cloud. I am working with a very basic MCU and do everything in raw bytes.
Also. Not in the documentation: There are two test modes. Mode 1, CTRL_REG4 = 04, moves the readings one way and Mode 2, CTRL_REG4 - 02, moves them the same amount in the opposite direction. Average the readings from both modes. If the answer is the regular reading (within two LSBs) then all is OK.
Now I am having fun (not) trying to reliably generate interrupts at 10 Hz ODR.
Rob
2021-01-27 8:05 AM