cancel
Showing results for 
Search instead for 
Did you mean: 

li2dw12, Does the "LP_MODE" value make effect, if high performance is set in the "MODE" of CTR1

MBoch.2
Associate II

We have following configuration in CTRL1: 

ODR[3:0]: 1001b (High-Performance / Low-Power mode 1600/200 Hz)

MODE[1:0]: 01b(High-Performance Mode (14-bit resolution))

And the value in the  "LP_MODE[1:0] " might be different depending on the state we came from. 

The question here does the value in the "LP_MODE[1:0] " have any affect in this configuration when high performance is selected in MODE[1:0]?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @MBoch.2 ,

If you select High performance Mode with the bits MODE [1:0] than leave the LP_MODE[1:0] at the default value so that the high performance configuration will not be affected.

If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @MBoch.2 ,

If you select High performance Mode with the bits MODE [1:0] than leave the LP_MODE[1:0] at the default value so that the high performance configuration will not be affected.

If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.