2024-06-21 4:16 PM
Trying to get the lowest power out of this device, but it seems to draw at least 900uA of current when even the accel and gyro are disabled. Any suggestions on how to get the current draw of this device lower? Here's my setup:
I can confirm that by removing the IMU the current drops to the expected 0.1mA. Any ideas as to why it's consuming so much current, relatively speaking?
2024-06-26 1:43 AM
Hi @NSmit.9 ,
Can you connect also SDA, SDO and SCL? And then measure the consumption in power down?
Thanks
2024-06-26 7:07 AM
Federica,
We currently have the following connected:
Was that what you were referring to? Also, a few other questions on signal connections:
Saving a couple of microamps here would be much appreciated.
2024-06-28 12:32 AM
Hi @NSmit.9 ,
You can refer to table 1 in datasheet:
It's ok to leave INT1 and INT2 floating if they are used as output, otherwise you should polarize them through a pull up.