cancel
Showing results for 
Search instead for 
Did you mean: 

IR STHS34PF80 - False motion detect on external envinronment (wind and/or sun)

socha6
Associate

Hello,

we use STHS34PF80 sensor as little animals detector (FOV ~ 20cm) and we have problem with false motion detection on outside. When we have sunny day the sensor goes crazy and output random MOT_FLAG signals. We have try to change LPF_P_M and LPF_M filters but without success. Also we try to change motion threshold and motion hysteresis also without success.
Is any solution for this problem?

Thanks in advance

Adam Socha

3 REPLIES 3
Federica Bossi
ST Employee

Hi @socha6 ,

Welcome to ST Community!

STHS34PF80 is based on IR technology and using it in outdoor applications you could have some unexpected IR reflections which cause more noise.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@Federica Bossi we know that, but we are looking for solution. We need to eliminate that problem.

We are a startup developing IoT devices. We are currently closing the prototype phase and starting mass production. Planned volume of devices - 20 million by the end of 2029.

Federica Bossi
ST Employee

Hi @socha6 ,

You should open a ticket to our online support so that they can help you for your specific case.

Here the link: https://ols.st.com/s/

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.