2011-01-15 10:31 PM
This board supports an ''AHRS'' mode, but on my computer the option is grayed out. I am running V2 of the board which is supposed to support this mode. Is there some addional firmware that must be loaded? If so, where do I get it and how do I load it?
Thanks Al2011-01-18 2:03 AM
Hi Al,
Probably firmware upgrading is necessary, here below the procedure:Press Leave DFU mode
iNEMOâ„¢ Team
2011-01-25 2:17 AM
Hi Fabio
I upgraded my iNemo STEVAL-MKI062V2 with the file ''iNEMOV2_Firmware_PackageV2.0.0_AHRS.dfu'', but the AHRS stays greyed out in the iNemo Suite GUI, any reason why we can't use the AHRS mode ? Regards Philip2011-01-26 6:06 AM
Hi Philip,
First, check about correct upgrading of firmware trought Help>About menu of Suite (with the board connected).
Below the versions of Suite Ver.2.0.0, as reference:
ControlLibrary Ver. 2.0.04
ControlLibrary.MKI062V2 Ver. 2.0.0
iNEMO 2 SDK for STEVAL-MKI062V2 Ver. 1.6.0
TL_002 Frame Transport Layer Ver. 1.0.0
PL_001 Dynamic Link Library Ver. 1.1.2
Firmware :iNEMO Firmware_Version_2.0.0 - iNEMO AHRS ENABLE V1.2.0
Hardware :iNEMO V2 Hardware_Version_1
After, you kindly follow this simple sequence:
1)
Connect the board to USB2)
Open the Suite and connect the board to the virtual COM (pag.8 of attached UM1010)3)
Push the Connect Icon the communication between Suite and Board(fig.10)4)
Set the acquisition mode to AHRS from Tools>Communication>Mode(pag.12)5)
Select the acquisition mode (sample/continuous) and push the Play Icon6)
Now all is ready for launch the 3D Demo cube in AHR mode Best Regards Fabio ________________ Attachments : UM1010.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzYJ&d=%2Fa%2F0X0000000bNX%2FUPRZyKrJbrnDG7UnLhCTFgsVszah1qZOFh4il4JfbmU&asPdf=false2011-01-26 11:30 PM
Thanks Fabio
Everything is working now! You need to be connected BEFORE you can change the mode !! Philip