cancel
Showing results for 
Search instead for 
Did you mean: 

In LSM6DSM, wrote a specific value to control registers. But gives different values from reading the same register.

SM.13
Associate

I'm using LSM6DSM sensor with the code from ST's github.I was able to read the whoamI register correctly. Then I wrote configuration(0x60) to the control registers(CTRL2_G) for gyro . When I read the same registers, it is always giving me a value of (0x02). These were all 0s at start. Also, the output registers like OUT_XL are giving 0 always.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @SM.13​ ,

that's strange... did you try to configure also the accelerometer (for example CTRL1_XL = 60h)?

And at which Vdd/VddIO are you working?

-Eleon