cancel
Showing results for 
Search instead for 
Did you mean: 

IIS3DWB offset calibration is missing

Pavel_Levkoev
Associate

Hello All,

is it normal that the data in the offset calibration registers disappears after a power restart?

 

 

2 REPLIES 2
Federica Bossi
ST Employee

Hi @Pavel_Levkoev ,

Welcome to ST Community!

Do you mean registers: 73h, 74h, 75h?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Yes exactly,  and register  CTRL6_C (15h) with USR_OFF_W bit.

at the moment, I have to save calibration values to non-volatile memory and set them every initialization. It seems to me that something is wrong here, because logically such calibration is mainly used for correction and displacement after soldering/assembly. I.e. ideally only once.