cancel
Showing results for 
Search instead for 
Did you mean: 

I want to get gps information using p nucleo lrwan1.

KKS
Associate II

I want to get gps information using p nucleo lrwan1. Can I get an open source that can help? I'll use the uart port.(gps)

1 REPLY 1
Legacy member
Not applicable

Hello,

I am afraid this is not possible. LoRa operates in EU at 868 MHz and 915 MHz in the US. However, GPS utilizes 1575.42 MHz (10.23 MHz × 154) called L1 and 1227.60 MHz (10.23 MHz × 120), called L2.

David