2019-12-05 01:54 PM
The datasheet also refers to self test modes, but no explanations are given.
2019-12-10 08:12 AM
2019-12-10 09:05 AM
Thank you very much. These documents are quite helpful.
Would I be correct to assume that the RMS noise numbers are in a 40 Hz band (ODR/2 = 80/2) and that they would be the same at FS=+/- 4 Gauss?
2019-12-11 06:14 AM
Right, but take care of the offset that is not small hand has to be measured and subtracted to the acquired data. It doesn't directly affect the rms noise however. Regards