cancel
Showing results for 
Search instead for 
Did you mean: 

I'm a beginner. and How can I start to learn about using MEMS microphone for Ultrasound condition based monitoring ?

PKata.1
Associate

Please, Help

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @PKata.1​ ,

From a general point of view, you might refer for to Application note AN5522, Ultrasound behavior and guidelines of analog MEMS microphone IMP23ABSU.

From an application point of view, for examples using the microphone in ultrasound way you can refer to the X-CUBE-MEMSMIC1: The package also includes an example of ultrasound condition monitoring (UltrasoundFFT) that calculates the FFT of the analog microphone signal and streams the result to a PC GUI via USB. The microphone sampling rate is set by default to 192 kHz whereas the microphone bandwidth is up to 80 kHz.

-Eleon

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @PKata.1​ ,

From a general point of view, you might refer for to Application note AN5522, Ultrasound behavior and guidelines of analog MEMS microphone IMP23ABSU.

From an application point of view, for examples using the microphone in ultrasound way you can refer to the X-CUBE-MEMSMIC1: The package also includes an example of ultrasound condition monitoring (UltrasoundFFT) that calculates the FFT of the analog microphone signal and streams the result to a PC GUI via USB. The microphone sampling rate is set by default to 192 kHz whereas the microphone bandwidth is up to 80 kHz.

-Eleon