cancel
Showing results for 
Search instead for 
Did you mean: 

I am about to develop my own firmware for STEVAL-MKI109V3 (with STEVAL-MKI159V1, which has the LSM9DS1). Could someone share source code a complete IOC file or even a complete demo app? If ST already sharing these, where do I find them? Thanks.

AKuru.1
Associate II

I am already able to build firmware, which blinks LEDs, but I would like to cut some corners.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @AKuru.1​ , you can find STEVAL-MKI109V3 .ioc file here.

If you just want to interface LSM9DS1 and STEVAL-MKI109V3 in a custom way, it is not difficult to start a new project on STEVAL-MKI109V3 from scratch: you can base on STM32CubeIDE and create a project for STM32F401VE MCU and enabling the appropriate interfaces as described by the STEVAL-MKI109V3 schematic.

If you want to control the Unico GUI, I suggest you to download the Unico lite source code, which enables you to modify part of the interface.

Regards

AKuru.1
Associate II