cancel
Showing results for 
Search instead for 
Did you mean: 

IIS2DULPX one shot setup

PedroArfeli
Associate

Hello 

I suspect I'm about to make a dumb question but I've been strugling for the past 2 days trying to just make a simple reading of the accelerometer. Just that get those values out of X, Y and Z axis...

I can get the correct responses out of the WHO_AM_I register and the status from the other setup registers. No matter what I do, the readings from registers 0x28~0x2D keep returning zero. I need help to understand what I may be doing wrong...

Code below:

 

 

#include <Arduino.h>
#include <Wire.h>

#define i2c_sda 8
#define i2c_scl 9
#define x_l 0x28
#define x_h 0x29
#define y_l 0x2A
#define y_h 0x2B
#define z_l 0x2C
#define z_h 0x2D

uint8_t addr;
uint8_t outx_l;
uint8_t outx_h;
uint8_t outy_l;
uint8_t outy_h;
uint8_t outz_l;
uint8_t outz_h;
uint16_t X;
uint16_t Y;
uint16_t Z;
uint16_t msb;
uint8_t data;

void setup() {
  // put your setup code here, to run once:
  Serial.begin(115200);
  Serial.println("\nI2C Scanner");
  delay(1000);
  Serial.println ("I2C scanner. Scanning ...");
  Wire.begin(static_cast<int>(i2c_sda), static_cast<int>(i2c_scl), static_cast<uint32_t>(100000));
  byte count = 0;
  for (byte i = 8; i < 120; i++)
  {
    Wire.beginTransmission (i);
    if (Wire.endTransmission () == 0)
      {
      Serial.print ("Found address: ");
      Serial.print (i, DEC);
      Serial.print (" (0x");
      Serial.print (i, HEX);
      Serial.println (")");
      count++;
      addr = i;
      delay (1);
      }
  }
  Serial.println ("Done.");
  Serial.print ("Found ");
  Serial.print (count, DEC);
  Serial.println (" device(s).");
  delay(1000);


   // Turn on the accl // ODR = 200 Hz, High-Performance
  Wire.beginTransmission(addr);
  Wire.write(0x10);
  Wire.write(0x64);
  Wire.endTransmission(true);

  // FS ±2 g, one-shot using interface
  Wire.beginTransmission(addr);
  Wire.write(0x14);
  Wire.write(0xF0);
  Wire.endTransmission(true);

 
}




void loop() {

  //sadw = addr << 1;
  //sadr = sadw | 1;
 
  delay(25);

  //-------------------------------------------------------------------
  Wire.beginTransmission(addr);
  Wire.write(x_l);
  Wire.endTransmission(false);
  Wire.requestFrom(addr, 1);
  if (Wire.available()) {
    outx_l = Wire.read();
  }
  Wire.endTransmission(true);
  delay(25);

  //get MSBs
  Wire.beginTransmission(addr);
  Wire.write(x_h);
  Wire.endTransmission(false);
  Wire.requestFrom(addr, 1);
  if (Wire.available()) {
    outx_h = Wire.read();
    Serial.println(outx_h, HEX);
  }
  Wire.endTransmission(true);
  delay(25);

  msb = outx_h;
  X = (msb << 8) | outx_l;
  Serial.println(X, HEX);
  delay(1000);
}
 
======================================================
 
and on platformio.ini:
[env:esp32-s3-devkitc-1-n16r8v]
platform = espressif32
board = esp32-s3-devkitc-1-n16r8v
framework = arduino

monitor_speed = 115200

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @PedroArfeli ,

Can you try to follow our official example on Github and let me know if you get results different from 0?

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @PedroArfeli ,

Can you try to follow our official example on Github and let me know if you get results different from 0?

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PedroArfeli
Associate

Thank you Federica. With the help of that example I was able to correctly configure the sensor.