2020-03-02 2:50 AM
hello,
i m trying to generate an interrupt event based on a defined threshold to wakeup the mcu from stop mode
here is my function to enable this feature
void LPS25_interrupt_Config(){
Conf_reg1 |= (LPS25HB_CTRL_REG1_PD | LPS25HB_CTRL_REG1_ODR_25HZ);
HAL_I2C_Mem_Write(&hi2c1,LPS25HB_ADDRESS_WRITE,LPS25HB_CTRL_REG1,1,&Conf_reg1,1,0xff);
Conf_reg2 = (LPS25HB_CTRL_REG2_AUTOZERO);
HAL_I2C_Mem_Write(&hi2c1,LPS25HB_ADDRESS_WRITE,LPS25HB_CTRL_REG2,1,&Conf_reg2,1,0xff);
Conf_reg3=(LPS25HB_CTRL_REG3_INT_S_Pressure_LH );
HAL_I2C_Mem_Write(&hi2c1,LPS25HB_ADDRESS_WRITE,LPS25HB_CTRL_REG3,1,&Conf_reg3,1,0xff);
Interrupt_conf= (LPS25HB_INTERRUPT_CFG_LIR );
HAL_I2C_Mem_Write(&hi2c1,LPS25HB_ADDRESS_WRITE,LPS25HB_INTERRUPT_CFG,1,&Interrupt_conf,1,0xff);
HAL_I2C_Mem_Write(&hi2c1,LPS25HB_ADDRESS_WRITE,LPS25HB_THS_P_L,1,&Threshold_L,1,0xff);
HAL_I2C_Mem_Write(&hi2c1,LPS25HB_ADDRESS_WRITE,LPS25HB_THS_P_H,1,&Threshold_H,1,0xff);
HAL_I2C_Mem_Read(&hi2c1,LPS25HB_ADDRESS_READ,LPS25HB_INTERRUPT_CFG,1,&Interrupt_conf,1,0xff);
Interrupt_conf|=(LPS25HB_INTERRUPT_CFG_PL_E | LPS25HB_INTERRUPT_CFG_PH_E);
HAL_I2C_Mem_Write(&hi2c1,LPS25HB_ADDRESS_WRITE,LPS25HB_INTERRUPT_CFG,1,&Interrupt_conf,1,0xff);
HAL_I2C_Mem_Read(&hi2c1,LPS25HB_ADDRESS_READ,LPS25HB_CTRL_REG1,1,&Conf_reg1,1,0xff);
Conf_reg1 |= (LPS25HB_CTRL_REG1_DIF_E );
HAL_I2C_Mem_Write(&hi2c1,LPS25HB_ADDRESS_WRITE,LPS25HB_CTRL_REG1,1,&Conf_reg1,1,0xff);
}
i m verifying the inetrrupt source register to check if an interrupt was generated but i get nothing
Any thoughts or suggestions on what I might be doing wrong, or have setup incorrectly.
thanks !
2020-03-18 9:28 AM
Hi @ATAYE.1 , which pressure threshold for the activation of the interrupt did you set? How did you configured the LIR bit in INTERRUPT_CFG (24h) register (p. 39 of the datasheet)? Regards
2020-03-21 9:28 AM
hello @Eleon BORLINI thank you for replying
I've set the pressure threshold to 2 ( THS_P_L=0x02 and THS_P_H=0 )
and the LIR bit to 1 ( INTERRUPT_CFG= 0x07 )
i tried to follow the Autozero mode example in the application note but i get nothing in the interrupt source register
2020-03-24 4:02 AM
Hi @ATAYE.1 , which physical event did you use to trigger the interrupt? A pressure blow or an altitude change? Regards
2020-03-24 8:45 AM
Hello @Eleon BORLINI thank you again for replying
I inserted the sensor in a balloon
and I press the ball to increase the pressure
i m using The STEVAL-IDI003V2 evaluation platform
Regards.
2020-03-24 9:57 AM
Hi @ATAYE.1 , please note that the LPS25HB can measure between 260 to 1260 hPa absolute pressure range, so it cannot be used to detect a pressure much greater than the atmospheric pressure. Which are the pressure levels you want to monitor? Regards
2020-03-24 11:54 AM
hello @Eleon BORLINI ,
i've set the threshold pressure to 1hPa
my probleme is that the sensor isn't generating any interrupt ,
is there any order in which i have to set the registers so this could work properly ?
or am I missing something when initializing the sensor?
if you could point me to an example where they use the thrueshold based interrupt i will be very grateful
Regards
2020-03-25 2:43 AM
Hi @ATAYE.1 , I believe you should set the pressure something like atmospheric pressure + threshold pressure...
Did you already check the LPS25HB examples available on Github repository?
/**
* @brief Set the threshold tmp used for pressure interrupt generation (hPA).
* @detail THS_P=THS_P_H&THS_P_L and is expressed as unsigned number.
P_ths(hPA)=(THS_P)/16.
* @param *handle Device handle.
* @param Pressure threshold in hPA
* @retval Status [LPS25HB_ERROR, LPS25HB_OK]
*/
LPS25HB_Error_et LPS25HB_Set_PressureThreshold(void *handle, int16_t P_ths)
{
uint8_t buffer[2];
buffer[0] = (uint8_t)(16 * P_ths);
buffer[1] = (uint8_t)(((uint16_t)(16 * P_ths)) >> 8);
if(LPS25HB_WriteReg(handle, LPS25HB_THS_P_LOW_REG, 2, buffer))
return LPS25HB_ERROR;
return LPS25HB_OK;
}
Regards