Skip to main content
Gk.1
Associate III
January 4, 2021
Solved

Hii...Using IKS01A3 sensor board with STM32WB55 is it possible to develop interface whether the person is in sitting or standing position

  • January 4, 2021
  • 1 reply
  • 719 views

..

This topic has been closed for replies.
Best answer by Eleon BORLINI

Hi @Gk.1​ ,

you could for example try the FP-SNS-MOTENVWB1 example package, where the Activity Recognition library is implemented (Middlewares\ST\STM32_MotionAR_Library). You could also try to set up also the MotionPE real-time pose estimation library of the X-CUBE-MEMS1, although this is not present in the Motenvwb package by default. You could connect the system to the Unicleo-GUI (which supports the MOTENVWB package) and plot the activity recognition results from the IKS01A3 board.

Please let me know if you are able to implement it.

-Eleon

1 reply

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
January 4, 2021

Hi @Gk.1​ ,

you could for example try the FP-SNS-MOTENVWB1 example package, where the Activity Recognition library is implemented (Middlewares\ST\STM32_MotionAR_Library). You could also try to set up also the MotionPE real-time pose estimation library of the X-CUBE-MEMS1, although this is not present in the Motenvwb package by default. You could connect the system to the Unicleo-GUI (which supports the MOTENVWB package) and plot the activity recognition results from the IKS01A3 board.

Please let me know if you are able to implement it.

-Eleon