2023-09-12 6:39 AM
Hello,
I am trying to count steps from a Poky linux. I have already a driver configured which can be used to get accelero and gyro data. I've seen on the LSM6DSL's datasheet that the register FIFO_CTRL2 (07h) can enable the step counter that can get in the register in 4Bh.
In the existing linux driver, that functionality is not implemented. Do you have a version of the driver where it is possible to use it ? Or any documentation or example to modify this driver ?
Thanks,
Arthur
2023-09-12 7:01 AM