2023-02-16 12:48 PM
Solved! Go to Solution.
2023-02-17 12:19 PM
Welcome, @FKara.3, to the community!
You should be able to use this function with all MCUs, because the MLC (Machine Learning Core) and the FSM (Finite State Machine) are integrated in the sensor and only need to be configured accordingly. You can find repositories for this under the above mentioned URLs.
Does it answer your question?
Regards
/Peter
2023-02-17 12:19 PM
Welcome, @FKara.3, to the community!
You should be able to use this function with all MCUs, because the MLC (Machine Learning Core) and the FSM (Finite State Machine) are integrated in the sensor and only need to be configured accordingly. You can find repositories for this under the above mentioned URLs.
Does it answer your question?
Regards
/Peter
2023-02-17 1:22 PM
Hello Peter,
Thank you for the answer. Yes, that was what I was looking for.
Kindly,
Fehmi