2022-09-20 8:20 AM
2022-09-21 3:19 AM
Welcome, @Nur ÃZã¶Ren, to the community!
On the website of the VL53L0X you have probably already found the references to hardware tools like e.g. X-NUCLEO-53L0A1 and the software package X-CUBE-53L0A1. The latter contains the drivers for STM32F4 and STM32L4, other STM32 families can be added relatively easily, which of course requires some changes in the source code.
Similar questions have already been asked in the community, e.g. here or there, with the search for X-CUBE-53L0A1 even more can be found.
Does it answer your question?
BTW: if the STM32F103C8T6 is on a board called Blue Pill, you should know that the STM32s installed there are usually counterfeits, i.e. not originals from STMicroelectronics. In many cases, they behave completely differently from the originals. So don't be surprised if something doesn't work as expected.
Regards
/Peter
2022-09-21 3:19 AM
Welcome, @Nur ÃZã¶Ren, to the community!
On the website of the VL53L0X you have probably already found the references to hardware tools like e.g. X-NUCLEO-53L0A1 and the software package X-CUBE-53L0A1. The latter contains the drivers for STM32F4 and STM32L4, other STM32 families can be added relatively easily, which of course requires some changes in the source code.
Similar questions have already been asked in the community, e.g. here or there, with the search for X-CUBE-53L0A1 even more can be found.
Does it answer your question?
BTW: if the STM32F103C8T6 is on a board called Blue Pill, you should know that the STM32s installed there are usually counterfeits, i.e. not originals from STMicroelectronics. In many cases, they behave completely differently from the originals. So don't be surprised if something doesn't work as expected.
Regards
/Peter
2022-09-21 3:35 AM
Yes, I got the answer to my question. I was also welcome. Thank you for your attention
2022-09-21 4:17 AM
Great!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.