cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L8CX Driver software download

parkescape
Associate II

Hi - when I attempt to download the driver for this device the download never completes; I get a file "Unconfirmednnnn.crdownload" in my download folder. I'm using Edge browser on a Windows 11 Home 64 bit operating system. Using Norton, can't see anything there that would prevent the download. Have successfully downloaded from other sites many times with no issues.

Anyone with any insights?

Thanks.

4 REPLIES 4
Peter BENSCH
ST Employee

Welcome @parkescape, to the community!

I have just been able to successfully download the available packages as a test. In your case, it could be an issue with a virus scanner that may be present and is not accepting your download. You could also try using a different browser (e.g. Firefox, Brave, Chrome) or another machine?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User

@parkescape wrote:

I get a file "Unconfirmednnnn.crdownload" in my download folder


Have you tried deleting that?

I sometimes find that the browser gets confused: it thinks it's already done this download, so doesn't try to do it again.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thanks - I tried the  download a few times with the same result. Eventually renamed the file to .zip  and was able to open it and access the files.

 

Regards

Thanks - I suspected the virus scanner but couldn't see anything that would stop the download and had no alerts from it. Eventually renamed the file to a .zip and that worked.

 

Regards