cancel
Showing results for 
Search instead for 
Did you mean: 

CS control LIS2DH

Artem777
Associate
In the project I use Attiny13a) + 
LIS2DH SPI interface.
One leg of the microcontroller is
missing.
Is it possible in SPI mode to
connect the CS pin directly to GND,
and not to the microcontroller port.
In I2C mode there are enough pins,
everything works fine, but the
current consumption is too high.

 

1 REPLY 1
Federica Bossi
ST Employee

Hi @Artem777 ,

What current consumption do you get that is too high?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.