cancel
Showing results for 
Search instead for 
Did you mean: 

Compiling on Atollic, or anything other than IAR ?!?

jake
Associate II
Posted on January 26, 2012 at 23:23

I can't get DFU or iNemo firmware code to compile with Atollic.

The code seems to be a mess with changes to the standard libraries, etc..  Please create a project file for Atollic, or tune up the code so it will compile on anything other than IAR, or help me with some instructions on how to accomplish this.

Please provide some support for Atollic/eclipse, otherwise you're shutting out ALL linux developers. 

#atollic
1 REPLY 1
jake
Associate II
Posted on January 27, 2012 at 00:52

I just tried using IAR workbench v6.30 and none of the iNemo/DFU code will compile.  

Apparently has to do with CMSIS version incompatibilities, which is why I gave up on IAR previously.