2024-11-20 1:55 AM - edited 2024-11-20 2:10 AM
Hi,
We are working with the LPS22DF pressure sensor to be used in our device adapting a 3.3V system and have encountered issues related to the interaction between VDD_IO, VDD, and the I²C bus.
When VDD_IO is powered but VDD is not:
We have tested it using the evaluation kit and also on a breadboard. What we did was add a diode between VDD and VDD_IO to temporarily eliminate the issue. However, the I²C lines are still not stable and show a "wavy" signal.
Do you have any suggestions or recommendations? This is the first time we have encountered this kind of behavior with an ST sensor. We do not want to use power-down mode, as we are required to maintain extremely low current consumption. Using a different power source is also not an option.
2024-11-22 12:23 AM
Appreciate if there is any guidance or recommendations
2024-11-25 11:59 PM - edited 2024-11-26 12:03 AM
I'm doubting that this is not the right channel to raise this topic?
2024-12-06 6:05 AM
Hi @Adi_Aljarbou ,
For safety during mounting and managing, all pins have two esd diodes (vs GND and vs its power supply). The two power supply lines have different strategy in terms of ESD but in any case they are intrinsically connected. This can avoid that the device is not correctly powered. The interaction between VDD and VDDIO is evident for this reason.
Our suggestion is to avoid to have only one power supply that can create instability as described before. Preferred solution is to put the device in power down (ODR @0000).