2023-12-11 06:14 PM
2023-12-12 04:31 AM
Hi @insist_66 ,
The BlueCoin can work at a maximum of 16kHz.
2023-12-12 05:51 AM
The audio signal is obtained from the digital MEMSM Kefeng as a 1-bit PDM signal, which is then converted into a 16 bit PCM sample by a PDM to PCM conversion filter at 16 kHz. Using the AcousticBF algorithm in FP-AUD-SMARTMIC1, can a sampling rate of 48KHZ be achieved
2023-12-14 06:30 AM
Hi @insist_66 ,
Unfortunately this is not possible: the library only works up to 16KHz, both input and output.
We don't have libraries or examples that from a 16KHz input signal would allow a 48KHz output signal.