2017-08-14 8:33 AM
Hi,
I'm using LSM6DSL and unable to operate X axis on accelerometer. The Y and Z axes give me the right results but X axis is stable at 32756 and changes only by 5 points. I have 4 devices with LSM6DSL and all behave same. Tested even without FIFO (same result). Because 4 devices do the same, I'm not sure of device fault.
Here is my setup:
/* Enable register address automatically incremented during a multiple byte
access with a serial interface. */LSM6DSL_ACC_GYRO_W_IF_Addr_Incr(NULL, LSM6DSL_ACC_GYRO_IF_INC_ENABLED); /* Enable BDU */LSM6DSL_ACC_GYRO_W_BDU(NULL, LSM6DSL_ACC_GYRO_BDU_BLOCK_UPDATE );// Low power enabled (XL_HM_MODE = 1)
LSM6DSL_ACC_GYRO_W_LowPower_XL(NULL, LSM6DSL_ACC_GYRO_LP_XL_DISABLED) ;/* Scale selection. */
LSM6DSL_ACC_GYRO_W_FS_XL(NULL, LSM6DSL_ACC_GYRO_FS_XL_4g );/* Set accelero FIFO decimation */
LSM6DSL_ACC_GYRO_W_DEC_FIFO_XL(NULL, LSM6DSL_ACC_GYRO_DEC_FIFO_XL_NO_DECIMATION); /* Set FIFO ODR to highest value */LSM6DSL_ACC_GYRO_W_ODR_FIFO(NULL, LSM6DSL_ACC_GYRO_ODR_FIFO_6600Hz);/* Set FIFO_FULL on INT2 */
LSM6DSL_ACC_GYRO_W_FULL_FLAG_on_INT2(NULL, LSM6DSL_ACC_GYRO_INT2_FULL_FLAG_ENABLED); /* Set FIFO watermark */LSM6DSL_ACC_GYRO_W_FIFO_Watermark(NULL, FIFO_WATERMARK); /* Set FIFO depth to be limited to watermark threshold level */ if(LSM6DSL_ACC_GYRO_W_STOP_ON_FTH(NULL, LSM6DSL_ACC_GYRO_STOP_ON_FTH_ENABLED);/* Set ODR at 104Hz */
LSM6DSL_ACC_GYRO_W_ODR_XL(NULL, LSM6DSL_ACC_GYRO_ODR_XL_104Hz);/* Set FIFO mode to Continuous */
LSM6DSL_ACC_GYRO_W_FIFO_MODE(NULL, LSM6DSL_ACC_GYRO_FIFO_MODE_DYN_STREAM_2);Thanks
Ondrej Meca
#lsm6dsl2017-08-21 1:13 AM
Hey,
Could you also post your reading scheme ? This might be of help to those who would like to help you debug