cancel
Showing results for 
Search instead for 
Did you mean: 

ASM330LHB chip shows large gyro bias jumps during temperature cycling (-40°C to 100°C)

dayu
Associate II

I performed a temperature cycle check on the ASM330LHB chip. Relative to the warming process (red curve), during the cooling process (blue curve), it is prone to large zero-bias jumps (in the red box of the picture)。

 

The jump during the cooling process, I feel like there is a correction mechanism in the gyro in the chip, which recognizes a large shift in the gyro zero bias during the cooling process, and then immediately corrects the large zero bias shift.

Can you please help explain what causes this?

Note: These data on the image have been smoothed for 10 seconds.

dayu_0-1707210744786.png

 

dayu_1-1707210985255.png

 

 

10 REPLIES 10

ok, thank you for reply.