2017-12-13 1:27 AM
Hi
I'm using LSM6DS3 for activity detection.The SLEEP_STATE_IA bit of the WAKE_UP_SRC register is used to monitor the activity/inactivity,
but I have noticed that the value for the bit remains the same(ie when sleep event is detected the value of SLEEP_STATE_IA is set to 1 but even when activity is detected the value remains the same)
Can you suggest a fix for the problem? OR provide an alternative for activity detection
2017-12-14 12:32 PM
Can you please provide your complete sensor configuration?
2017-12-18 10:22 PM
Please find the sensor pseudocode in the attachments.
Other than the above-mentioned problem, I'm facing trouble with the orientation change.
When the sensor is shaken it detects an orientation change rather than activity. Please provide a solution to this problem too.
2017-12-22 1:47 AM
Maybe, he cannot upload detail register values.
How do you upload example full register values about the wanted operation registers (read '1' of
SLEEP_STATE_IA bit
during sleep status after inactivity).
I try to set and read SLEEP_STATE_IA bit in LSM6DSL.
Successfully, read '1' of SLEEP_STATE_IA bit during sleep status after inactivity.
but, I fail to read '1' of
SLEEP_STATE_IA bit in LSM6DS3. (always read '0' of
SLEEP_STATE_IA bit)
(same setting values of LSM6DSL)So, I want to know it too. how do i set in LSM6DS3 . (just want sample setting register values in
LSM6DS3
or STEVAL-MKI160V1 (LSM6DS3 EV kit))