2023-12-12 12:39 AM
Can the AcousticBF beamforming algorithm from FP-AUD-SMARTMIC1 algorithm be used on the entry-level kit of BlueCoin board (STEVAL-BCNCS01V1) to achieve audio acquisition at a sampling rate of 48kHz?
2023-12-12 4:31 AM
Hi @insist_66 ,
Welcome to ST Community!
The library AcousticBF can't work at 48KHz
2023-12-12 5:52 AM
The audio signal is obtained from the digital MEMSM Kefeng as a 1-bit PDM signal, which is then converted into a 16 bit PCM sample by a PDM to PCM conversion filter at 16 kHz. Using the AcousticBF algorithm in FP-AUD-SMARTMIC1, can a sampling rate of 48KHZ be achieved
2023-12-13 1:43 AM
Hi @insist_66 ,
I think there is a misunderstanding: the library only works up to 16KHz, both input and output.
We don't have libraries or examples that from a 16KHz input signal would allow a 48KHz output signal.