cancel
Showing results for 
Search instead for 
Did you mean: 

Achieving < 1ug/√Hz at 1 Hz using ADXL355 module

shahriar193
Associate II

Is there any way to achieve this desired noise sensitivity using the ADXL3555 accelerometer. Maybe using filter? Appreciate the help.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @shahriar19, to the community!

You took a slight wrong turn in your search for support for your MEMS sensor: STMicroelectronics also has such sensors in its range, but the ADXL3555 is not a product of STMicroelectronics, so it is unlikely that anyone here can help you.

Good luck! /Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @shahriar19, to the community!

You took a slight wrong turn in your search for support for your MEMS sensor: STMicroelectronics also has such sensors in its range, but the ADXL3555 is not a product of STMicroelectronics, so it is unlikely that anyone here can help you.

Good luck! /Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you for your answer. Can you suggest any sensor that has noise sensitivity of < 2ug/√Hz at 1 Hz. The frequency range can be 1 to 100 Hz. Any suggestions will be appreciated.