2013-08-09 2:45 PM
I have purchased the STEVAL-MKIO62v2 evaluation kit and I am looking for the source code so I can rebuild the firmware for this board. Essentially I need the source code for the RTOS that goes on the MCU as well as the code to access all of the on board sensors (MEMS, TEMP, PRESSURE sensors).
#inemo-stm32-stm32f10xxx-firmware2013-09-07 3:44 AM
http://www.st.com/web/catalog/tools/FM147/CL1818/SC1528/PF252510
I think requests need to be pushed in via local ST reps and FAEs2013-11-22 11:37 AM
Hello,
How to download the iNEMOEngine_LI3 source code? There is no download link in this website.Yujia