cancel
Showing results for 
Search instead for 
Did you mean: 

Will the ST67W611M have BLE TMAP audio support?

ifa8
Associate

hiii,

Do you plan to support BLE TMAP on this module?

 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @ifa8, to the community!

The ST67W611M1 is not intended for TMAP/LE Audio and does not include the requirements such as LE isochronous channels, host stack with generic audio framework, ASCS/PACS, or LC3 Codec.

However, you can use it as an NFC Secure Element and/or BLE Secure Element in a system solution with an LE Audio-capable host MCU/BLE radio chip that then implements TMAP, for example, the STM32WBA.

Does this answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @ifa8, to the community!

The ST67W611M1 is not intended for TMAP/LE Audio and does not include the requirements such as LE isochronous channels, host stack with generic audio framework, ASCS/PACS, or LC3 Codec.

However, you can use it as an NFC Secure Element and/or BLE Secure Element in a system solution with an LE Audio-capable host MCU/BLE radio chip that then implements TMAP, for example, the STM32WBA.

Does this answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.