cancel
Showing results for 
Search instead for 
Did you mean: 

bluenrg2 DTM_UART.hex can not running

mfc4143
Associate

I use DTM project,download to my board,but it is not running.I use my project it can running normal.How to solve it ,thanks

1 REPLY 1
Dominique FOLLEZOUR
ST Employee

Hello

Could you elaborate a bit more about setup:

Your own PCB is based on BlueNRG-2 chipset or BlueNRG-M2SP/SA  ?

If chipset what is your HW configuration : external 32Khz , RO ? SMPS ?

When flashing DTM you are then willing to connect yo board using BlueNRG GUI over UART ? and connection failed ? If so, the UART mapping on your PCB is same as DTM sample code ?

Thanks

Br

Dominique