cancel
Showing results for 
Search instead for 
Did you mean: 

WIFI DIRECT MODE and 3G/4G connectivity

Don david
Associate II
Posted on April 11, 2017 at 12:12

Hi All,

I need some suggestion regarding my project.

I want  my device to send data in wifi direct mode to the Android device which has 3g/4g connectivity.The Android device  will then forward the data to the server , so that live tracking happens.

Can Anybody tell how to proceed with this

Kind Regards

Don David

#android #wifi-direct
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gerardo GALLUCCI
ST Employee
Posted on April 11, 2017 at 18:56

Hi David,

ST SPWF0xS modules are not implementing WiFi Direct mode. You can setup the ad-hoc mode, called IBSS into datasheet and user manuals. Or, better, use the miniAP capability. You can setupSPWF module to act as a basic AP, providing link up to 5 devices. Also DHCP/DNS servers are running in this case!

Please refer to this discussion:

https://community.st.com/0D50X00009XkY8pSAF