2018-09-14 4:31 PM
After the call returns BLE_STATUS_SUCCESS, but the target BLE Peripheral slave device stops advertising forever (i.e. a race between scan result, connection request and peripheral stop advertising/go out of range)?
It would be nice if a connection request timed out in a similar way to how a general scan times out (with a GAP procedure complete, 0x02). Now I have to babysit the BlueNRG-MS with my own timer after making a connection request - is there an easier way?
Thanks,
2018-12-20 2:07 PM
I have come across the same issue and agree with Scott that it would be nice if the connection request timed out rather than trying forever.
2021-02-08 10:07 AM
@nick239955_stm1_st and @Scott L�hr I agree - how did you end up terminating the attempted connection? Is there a function or a call back that will just make it stop and recover? I cant do a thing once it is waiting to connect!
Any help would be greatly appreciated