cancel
Showing results for 
Search instead for 
Did you mean: 

What settings are needed for client to resolve miniAP host name

markb
Associate II
Posted on July 27, 2015 at 16:23

Hi,

When the SPWF01 is in miniAP mode what setup will allow the client to resolve the module's domain name. Do I need to set ip_dns to be the module's IP address ?

Thanks,

Mark
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gerardo GALLUCCI
ST Employee
Posted on July 27, 2015 at 17:13

Hi Mark,

variable called ''ip_use_dhcp'' enables miniAP to run both dhcp and dns server feature. Clients (up to 5) can ask for ''ip_apdomainname'' resource, and miniAP can resolve that address to IP address.

j