2020-04-01 04:09 PM
I desgined custom board with bluenrg-ms which I bought in the mouser.com.
Therefore, I can't figure out what firmware the ic has.
My first reference is sensortile.
Because the schematic is very simple compare to the development kit.
Currently, my board is not working.
(I'm still looking for the reason)
So there is one question.
Which is better design for bluenrg-ms between sensortile and development kit?
2020-04-03 11:07 PM
Please look at designs based on module, for example X-NUCLEO-IDB05A1.
Using a module can be faster and easier to make the design work