2016-08-15 06:37 PM
Using BlueNRG 6.4b, I received an event that I think is Evt_Blue_Gatt_Procedure_Timeout (FF 05 02 0C 01 08 00). Document UM1755 says there should be 2 bytes after the event code but I'm seeing 3 on my SPI analyzer. Am I interpreting the event correctly?
2017-01-10 07:04 AM
Hi,
i'm using the BlueNRG with the firmware 6.4 with a smartphone application that send indications to the blueNRG (Slave), and after a delay, the BlueNRG send this event to my embedded application ... do you have an idea on why this event is generated ? in the documentation they say 'This event is generated by the client/server to the application on a GATT timeout (30 seconds).' but 30 seconds before, nothing happens, the BlueNRG is receiving indications and it acknowledges every indication received.
Thanks,
Mehdi