2023-10-19 6:33 PM
Hi, Is it possible to set the address of the transmitter or receiver via S2_LP DK? My project involves sending data via s2-lp between two sets (nucleo-l053r8 with steval-fki868v2), I would like to set one for receive only and the other for read only. Thanks in advance
2023-10-25 6:12 AM
Hello,
When you want to send a packet, use S2LPSetRxSourceReferenceAddress to set the receiver address (in the packet) and S2LPSetMyAddress to set the sender address