2022-08-14 01:13 AM
I'm working with (still) IDB011V1. There is an issue with using SWD connection to BlueNRG-LP. I can connect to the device via SWD, when the device is erased via UART, but after I flash the BlueNRG-LP, I can't connect it via SWD anymore.
Any solution for it?
******MASS ERASE OPERATION******
Mass Erase Boards: COM8 (ST DK)
10:01:56.838: Device COM8 (ST DK) -> Mass Erase: Started
10:01:58.548: Device COM8 (ST DK) -> Mass Erase: Finished
10:01:58.548: Device COM8 (ST DK) -> Mass Erase: Flash memory successfully erased.
******START FLASH OPERATION******
Flash Boards: COM8 (ST DK)
10:02:33.064: Device COM8 (ST DK) -> Device Identification
10:02:34.406: Device COM8 (ST DK) -> Flash Programming...
10:02:36.414: Device COM8 (ST DK) -> Flash Programming: SUCCESS.
10:02:36.438: Device COM8 (ST DK) -> Flash Memory Verifying...
10:02:39.422: Device COM8 (ST DK) -> Flash Memory Verifying: SUCCESS.
******END FLASH OPERATION******
******FLASH READ OPERATION******
Read of n.1 device connected by SWD (ST-Link/V2, CMSIS-DAP, J-Link)
10:02:47.741: Waiting device to read (device connected by CMSIS-DAP) ->FAILED. (It's not possible to connect to the device)
******MASS ERASE OPERATION******
Mass Erase Boards: COM8 (ST DK)
10:03:00.834: Device COM8 (ST DK) -> Mass Erase: Started
10:03:02.531: Device COM8 (ST DK) -> Mass Erase: Finished
10:03:02.531: Device COM8 (ST DK) -> Mass Erase: Flash memory successfully erased.
******FLASH READ OPERATION******
Read of n.1 device connected by SWD (ST-Link/V2, CMSIS-DAP, J-Link)
10:03:08.133: Waiting device to read (device connected by CMSIS-DAP) ->Device Connected
10:03:09.345: Device Identification -> BlueNRG-LP
10:03:10.444: Read Flash Memory -> SUCCESS
10:03:12.528: Device Disconnection -> SUCCESS
******FLASH OPERATION******
Flash of n.1 device connected by SWD (ST-Link/V2, CMSIS-DAP, J-Link)
10:03:27.531: Device connection by CMSIS-DAP -> Device connected
10:03:28.641: Device Identification -> BlueNRG-LP
10:03:29.707: Device Flash Programming -> SUCCESS (Flash Programmed in 2.763541 sec.)
10:03:32.471: Flash Verify Operation -> SUCCESS
10:03:33.783: Device Disconnection -> SUCCESS
10:03:35.484: Flash operation finished!
******END FLASH OPERATION******
******FLASH READ OPERATION******
Read of n.1 device connected by SWD (ST-Link/V2, CMSIS-DAP, J-Link)
10:03:39.981: Waiting device to read (device connected by CMSIS-DAP) ->FAILED. (It's not possible to connect to the device)
2022-08-16 04:54 AM
Hello,
I guess it could be related to the use of PA10.
When a FW is flashed having sleep mode enabled, SWD interface is disabled.
So you should enter bootloader mode in order to use SWD.
Bootloader is activated by hardware by forcing PA10 high during hardware reset
So you can use
Regards
Laurent
2022-08-16 10:25 AM
Thank you, Laurent - it works like you explained, and it also works fine with my custom board 🙂