STM BlueNRG-MS Max Characteristic length limited to 255 due to aci_gatt_add_char function limitations.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-05 11:23 PM
My general understanding is that the BLE standard supports characteristics with a lenght of up to 512 bytes. I'm using the BlueNRG-MS chip from STM but there the function call to add a characteristic has a uint8_t value for the length parameter
tBleStatus aci_gatt_add_char(uint16_t serviceHandle,
uint8_t charUuidType,
const uint8_t* charUuid,
uint8_t charValueLen,
uint8_t charProperties,
uint8_t secPermissions,
uint8_t gattEvtMask,
uint8_t encryKeySize,
uint8_t isVariable,
uint16_t* charHandle);
So this would allow only a maximum characteristic length of 255 bytes. According to this document the stack itself supports 2 bytes with FW 7.2 or higher. I have 7.23 so this should be fine but I cannot find any reference or example of a BlueNRG-MS middleware that would support a call with
charValueLen
of type
uint16_t
. I also downloaded the latest STSW-BLUENRG-DK and the examples also only support
uint8_t charValueLen
.
- Labels:
-
Low Power RF Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-07 10:21 PM
Please manually modify the parameter accordingly.
in bluenrg_gatt_aci.h:
tBleStatus aci_gatt_add_char(uint16_t serviceHandle,
uint8_t charUuidType,
const uint8_t* charUuid,
uint16_t charValueLen,
uint8_t charProperties,
uint8_t secPermissions,
uint8_t gattEvtMask,
uint8_t encryKeySize,
uint8_t isVariable,
uint16_t* charHandle);
in bluenrg_gatt_aci.c:
tBleStatus aci_gatt_add_char(uint16_t serviceHandle,
uint8_t charUuidType,
const uint8_t* charUuid,
uint16_t charValueLen,
uint8_t charProperties,
uint8_t secPermissions,
uint8_t gattEvtMask,
uint8_t encryKeySize,
uint8_t isVariable,
uint16_t* charHandle)
{
struct hci_request rq;
gatt_add_serv_rp resp;
uint8_t buffer[26];
uint8_t uuid_len;
uint8_t indx = 0;
serviceHandle = htobs(serviceHandle);
Osal_MemCpy(buffer + indx, &serviceHandle, 2);
indx += 2;
buffer[indx] = charUuidType;
indx++;
if(charUuidType == UUID_TYPE_16){
uuid_len = 2;
}
else {
uuid_len = 16;
}
Osal_MemCpy(buffer + indx, charUuid, uuid_len);
indx += uuid_len;
charValueLen = htobs(charValueLen);
Osal_MemCpy(buffer + indx, &charValueLen, 2);
indx += 2;
buffer[indx] = charProperties;
indx++;
buffer[indx] = secPermissions;
indx++;
buffer[indx] = gattEvtMask;
indx++;
buffer[indx] = encryKeySize;
indx++;
buffer[indx] = isVariable;
indx++;
Osal_MemSet(&resp, 0, sizeof(resp));
Osal_MemSet(&rq, 0, sizeof(rq));
rq.ogf = OGF_VENDOR_CMD;
rq.ocf = OCF_GATT_ADD_CHAR;
rq.cparam = (void *)buffer;
rq.clen = indx;
rq.rparam = &resp;
rq.rlen = GATT_ADD_CHAR_RP_SIZE;
if (hci_send_req(&rq, FALSE) < 0)
return BLE_STATUS_TIMEOUT;
if (resp.status) {
return resp.status;
}
*charHandle = btohs(resp.handle);
return 0;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-08 6:42 AM
Thanks, I'll give it a try! I assume the same modification applies for aci_gatt_update_char_value()?
What confuses me a bit though is that if this is the fix, then I assume the buffer content would have been incorrect so far right? Or does it distinguish between buffer of size 25 and size 26 to determine whether I have 1 or 2 byte charValueLen?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-09 5:51 AM
I did the modification but when I do
ret = aci_gatt_add_char(serviceHandle, UUID_TYPE_128, uuid, 470, CHAR_PROP_READ, ATTR_PERMISSION_NONE, GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP, 16, 0 , &charHandle);
I get return value 0x1F, so it fails to add the characteristic.
Did I miss something? What is the origin of this Osal_MemSet? My code uses BLUENRG_memcpy instead, is that a problem?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-11 7:16 PM
0x1F would be out of memory.
Please check the the "Max_Attribute_Records" value in your previous call to aci_gatt_add_serv().
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-11 11:18 PM
Thanks for your reply. That was my initial thought as well, but I already have it set to 30 with only 2 characteristics added. If I reduce the size of the characteristic to 250, it works. Any other idea how to fix that? Regarding the "max_attribute_records", is there a clarification how to get the number of attributes of a service?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-12 8:12 PM
A characteristic needs at least 2 attributes (1 for declaration and 1 for value).
It requires 1 additional attribute if the characteristic has the Notify (/Indicate) property, and 1 additional attribute for each descriptor.
In your service, normally the number of attributes you are going to need = 1 for service + 2 for *2 characteristics = 5 attributes
If you only need 1 connection in the application, please use "MODE 2" for the stack, as it reserves more memory (700 bytes) for characteristics records array size.
Please modify IFR to change the mode.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-13 12:41 AM
But as it works with characteristic size of 250 I assume it's not an issue with the "max_attribute_records"? Any other Idea how I can troubleshoot this? This is a rather urgent project and I either need to solve this issue or reduce my characteristic size - I prefer the first one... :)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-15 7:14 PM
>But as it works with characteristic size of 250 I assume it's not an issue with the "max_attribute_records"?
No. I was just clarifying the minimum requirement on the number of attributes parameter. And it looks you've configured a number more than enough.
>I either need to solve this issue or reduce my characteristic size - I prefer the first one
Your customized service and characteristics consume memory = 4 + (4 + 250) + (4 + 250) = 512 bytes (in case of no descriptors)
This seems to be a reasonable limit for stack MODE4, which reserves 590 bytes the characteristics records array.
You will need to configure the stack to MODE2 instead to have a larger memory for your characteristics.
Please modify IFR.
Release Notes for BlueNRG, BlueNRG-MS Stacks:
file:///C:/Program%20Files%20(x86)/STMicroelectronics/BlueNRG%20DK%202.0.2/Docs/bluenrg_fw_stack_release_notes_html/_blue_n_r_g-_m_s__stack_v7_2_c.html
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-16 3:16 AM
Actually the IFR is already set to MODE2