2023-03-06 12:22 AM
Solved! Go to Solution.
2023-03-06 7:40 AM
Welcome, @SBart.5, to the community!
Electrolytic capacitors are usually preferred at this point for price reasons. Using MLCC instead should not be a problem, but MLCC, especially when connected in parallel, usually have a much lower ESR than electrolytic capacitors, which can lead to large peak currents when switching on and possibly exceed the KNX limits. If necessary, this can be achieved by adding a series resistor.
Does it answer your question?
Regards,
/Peter
2023-03-06 7:40 AM
Welcome, @SBart.5, to the community!
Electrolytic capacitors are usually preferred at this point for price reasons. Using MLCC instead should not be a problem, but MLCC, especially when connected in parallel, usually have a much lower ESR than electrolytic capacitors, which can lead to large peak currents when switching on and possibly exceed the KNX limits. If necessary, this can be achieved by adding a series resistor.
Does it answer your question?
Regards,
/Peter
2023-03-06 8:04 AM
Thank you for your quick reply, that answers my question.
In our case we do not have enough space in the height for an electrolytic capacitor, so we need an alternative.
Regards, Sebastian
2023-03-06 8:07 AM
Great!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter