cancel
Showing results for 
Search instead for 
Did you mean: 

ST67W611M1: low accuracy of SNTP

nicolas
Senior II

I'm using the ST67W6X_MQTT example on a NUCLEO-U575ZI-Q and i got the following result:

04/11/2025 16:11:02.217 [RX] - SNTP Time: Tue Nov 04 16:11:03 2025
04/11/2025 16:11:27.886 [RX] - SNTP Time: Tue Nov 04 16:11:27 2025
04/11/2025 16:11:46.452 [RX] - SNTP Time: Tue Nov 04 16:11:48 2025
04/11/2025 16:12:02.734 [RX] - SNTP Time: Tue Nov 04 16:12:05 2025
04/11/2025 16:12:20.904 [RX] - SNTP Time: Tue Nov 04 16:12:21 2025
04/11/2025 16:12:37.945 [RX] - SNTP Time: Tue Nov 04 16:12:38 2025
04/11/2025 16:12:54.605 [RX] - SNTP Time: Tue Nov 04 16:12:57 2025
04/11/2025 16:13:12.778 [RX] - SNTP Time: Tue Nov 04 16:13:15 2025
04/11/2025 16:13:30.028 [RX] - SNTP Time: Tue Nov 04 16:13:30 2025
04/11/2025 16:13:49.107 [RX] - SNTP Time: Tue Nov 04 16:13:49 2025
04/11/2025 16:14:05.867 [RX] - SNTP Time: Tue Nov 04 16:14:09 2025
04/11/2025 16:14:23.925 [RX] - SNTP Time: Tue Nov 04 16:14:24 2025

this correspond to an error of: +1, +0, +2, +3, +1, +1, +3, +3, +0, +0, +4, +1

I was expecting errors of under a second.

--------------- ST67W6X info ------------
ST67W6X MW Version: 1.1.1
AT Version: 1.0.0
SDK Version: 2.0.89
Wi-Fi MAC Version: 1.6.44
BT Controller Version: 1.6.112
BT Stack Version: 1.9.56
Build Date: Sep 4 2025 11:32:47
Module ID: C6AFDBD111400004 (-B)
BOM ID: 1
Manufacturing Year: 2024
Manufacturing Week: 47
Battery Voltage: 3.302 V
Trim Wi-Fi hp: 6,6,6,6,6,6,5,5,5,5,6,6,6,6
Trim Wi-Fi lp: 5,6,6,7,7,8,8,8,8,8,9,9,9,9
Trim BLE: 5,4,4,5,6
Trim XTAL: 37
MAC Address: 40:82:7b:00:22:ce
Anti-rollback Bootloader: 0
Anti-rollback App: 0

6 REPLIES 6
Andrew Neil
Super User

Where does the RX timestamp come from? How accurate is it?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

From my computer, it should be accurate enough.

Having an error difference of 4s in less than 20s is extremely unlikely from the PC side (if it is the case, i should have easily detected it).

mbarg.1
Lead

You need to trim RTC and you can easily keep your local clock within 16/256 of second using SNTP - of course some additional coding required - more exact sincronization is possible but would waste a lot of resources.

PAY attention to SNTP server - some have large drift.

Maybe i didn't explain clearly how i got my results. Each line was obtain after restarting the firmware, so it's not a problem of the STM32 RTC.

I see - you are asking why MQTT does not sync better than that - SNTP in stratum 0,1,and 2 is by sure better than that, with SNTP I get better less than 1 second after first (coarse) syncronization, but i am using a task with SNTP to do it. Probably someone from MQTT can reply or you can reverse engineer the code to see how they get a sync from a UDP packet that has picoseconds precision time stamp with Stratum 0 reference.

An easy test could be to use wireshark and grab SNTP packets - you easily see what can be the loop delay between query and reply - precision acheavable is better than loop delay with zero effort.

I'm using the MQTT example only because it's the only example with SNTP.

I can't see the traffic because it's all done inside the ST67, the driver just send an AT request "AT+CIPSNTPTIME?" to get the time.